Solid Edge Creating Counterbore Holes in a Sheetmetal Bend

2022-03-11T08:53:29Z
PART/SHEETMETAL

Summary


Details

Placing a counter bore hole in a sheet metal bend or a plastic zone of the bend is not available using the standard hole command with counter bore option in earlier Solid Edge versions.

In this tutorial we will go through an alternate solution using the bend and unbend command in the ordered environment as well as the flatten pattern command. 

Solution



In this tutorial we will go through an alternate solution using the bend and unbend command in the ordered environment as well as the flatten pattern command. 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V220.0
Function: FEATURES

Ref: 002-8518422

KB Article ID# PL8518422

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN