Solid Edge The requested file is opened exclusively and cannot be accessed at this time.

2021-10-06T23:57:37Z
PART/SHEETMETAL

Summary


Details

One user is getting an error message, "The requested file is opened exclusively and cannot be accessed at this time." Other users can open Solid Edge files from the same location without problems.



Solution

This could be caused by a "stale" network drive. Somehow, the way it was mapped, it pointed to an older address. In this case, the IT specialist reconfigured the network drive so that it points to the most recent address and this solved the problem.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V219MP9
Function: FILE

Ref: 001-9906566

KB Article ID# PL8517791

Contents

SummaryDetails

Associated Components

PART/SHEETMETAL: FLAT_PATTERN