NX MCD: Send Signals to SIMIT raised error -2147467259
2021-10-06T23:27:48Z
Summary
Details
When a MCD-assembly is loaded in NX, and "SIMIT plug-in" function "Send Signals to Simit" is used then an error is raised in SIMIT:NX Error Message received!(-2147467259) External Component has thrown an exception.
Solution
Do NOT use assembly load options "Minimal Loading" but instead e.g. "Fully Load". Find this in NX under File --> Assembly Load Options --> Scope --> Option="Fully Load"
Notes and References
The SIMIT MCD Add-in is part of SIMIT (10.2) and need additional configuration to become available in the NX user interface.