For example after postprocessing a CAM operation in NX and generating a ptp file maybe you want to import the associated files generated into Teamcenter.
Solution
In order to import associated files into Teamcenter there is a customer default setting that controls it.
This setting will activate the popup menu in NX when saving the item, allowing you to choose if you want to import the associated files and which one do you want to import.
In this case a ptp file created in NX CAM after postprocessing a toolpath.
So, after importing the ptp file, you'll find it under named references under the UGMaster of the item in Teamcenter
Once the setting in customer defaults is activated, the popup menu allowing to import associated files cannot be deactivated for an specific Item (local preference does not exist), so everytime you create a new associated file and save the part the popup will appear.
The only way to deactivate it is going the temp folder of your NX installation , find the folder with the name of your item type and deleted associated files in the folder to avoid the fact of being identified as import.
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: CAM Version: V1930 Function: TC_MFG