Option to customize ribbon bar icon buttons (large/small).

2021-10-06T23:57:36Z

Summary


Details

Is there an option to customize ribbon bar icon buttons (large/small)?



Solution

Right click in the ribbon and choose 'Customize the Ribbon'.  In the CUSTOMIZE window, click on the Ribbon tab; then right click on any of the items in the right-hand pane (Home, Surfacing, etc.).  At the bottom of this short cut menu, select 'Button Options', then select use Large (or small) buttons.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V110MP9
Function: CMDRIBBON

Ref: 001-9907610

KB Article ID# PL8517602

Contents

SummaryDetails

Associated Components