How to open multiple sessions of the same NX version through Teamcenter

2021-10-06T23:27:48Z

Summary


Details

How to open multiple NX sessions (that are the same version) through Teamcenter. 
Many times, multiple sessions of NX are needed, but Teamcenter will only launch one NX session.



Solution

This can be done by modifying the start_nxmanager.bat file that is called when launching NX. 
1. Open the %TC_ROOT%\portal\start_nxmanager.bat file in a text editor. 
2. Modify the following line from: 
start "Teamcenter Integration for NX" /B "%UGII_ROOT_DIR%\ugs_router" -ugm -enable_cancel -version=%VERSION% %* 
to: 
start "Teamcenter Integration for NX" /B "%UGII_ROOT_DIR%\ugraf.exe" -pim=yes -ugm -enable_cancel -version=%VERSION% %*


The ugs_router.exe checks to see if there is already an NX session running. If there is a session running it will not open a new session. Modifying the line so that ugraf.exe will be called allows multiple sessions of NX to be launched from Teamcenter.


NOTE: Modifying this line could cause the user to login each time NX is launched. If this happens, it can be remedied by adding the username, password, and group to the statement in the start_nxmanager.bat file: 
start "Teamcenter Integration for NX" /B "%UGII_ROOT_DIR%\ugraf.exe" -pim=yes -u=<username> -p=<password> -g=<group> -ugm -enable_cancel -version=%VERSION% %*



Notes and References


Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: TC_PORTAL

Ref: 001-9902327

KB Article ID# PL8517064

Contents

SummaryDetails

Associated Components