Tecnomatix End of Support for Resource Browser module in Process Simulate on Teamcenter and Process Designer

2021-10-07T00:16:09Z
Process Simulate eM-Server

Summary


Details

Starting with Tecnomatix V16.1, the Resource Browser module will not be supported for Tecnomatix products.

The following products are impacted:


  1. Process Simulate on Teamcenter - Resource Search application within Teamcenter Manufacturing Access module can be used instead.
  2. Process Designer with CC integration - Exchanging resources from Teamcenter to eM-Server will be supported only via the generic mechanism of creating a sync request.



SFB-TECNOMATIX-8516948
Product Information:
  • Product: TECNOMATIX , Application: PROCESS_SIMULAT , Version: V16.1
  • Product: TECNOMATIX , Application: EM-SERVER , Version: V16.1

KB Article ID# PL8516948

Contents

SummaryDetails

Associated Components

eMS/Tc/TcMA