Cloning a file using tcin_import raises "A token was found in a log file which is unknown or not valid at that point"

2021-10-06T23:27:48Z

Summary


Details

User has a case where using tcin_import with a clone file and needs to assign the part name with a double quote.  The string starts with a double quote and then adds a 2nd double quote to define an inch value in the part name.i.e  "1/2" hex head" and ends with a double quote. So there are 3 double quotes in the string, this raises the following error;

       "A token was found in a log file which is unknown or not valid at that point. on line number ##"


Solution

For this case, if you open the clone log file that was used in the tcin_import, in line number 29 you will see where the part file name that contains an inch value 1/2".

To fix this add a backslash before the double quotes for the inch value. Open the clone log in an editor and change line for the Part Name from "1/2" Hex Head" to "1/2\" Hex Head"  and the import will work without error.





Hardware/Software Configuration

Platform: na
OS: all
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V10.0.3
Function: CLONE_IMPORT

Ref: 002-8516679

KB Article ID# PL8516679

Contents

SummaryDetails

Associated Components