In SEDM user not able to configure one step workflow.

2021-10-06T23:57:33Z

Summary


Details

While releasing file only quick release workflow is active. One-step work flow is deactivated.
Unable to add non-Active directory users in SEDM one step workflow.

Solution

About non Active Directory users while configuring the One step workflow.
The Windows user and his email ID can be added directly (even though it shows 'Warning: User not found in active directory').
 
Steps:
Solid Edge Options -> Manage -> Workflow
Click on [Add] button
Enter 'User Information'
Windows User: - Uses name that you used to login in Windows
Email Address: -The email address should be type manually for non-Active Directory users. In case of Active Directory user, it will take email address automatically).
 
This user information will get added to 'Workflowsettings.txt file'. The default location is \Program Files\Siemens\Solid Edge 2020\Preferences. To select a Workflowsettings.txt file from another location, use the browse button.

Notes and References

9831119

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEDM

Ref: 002-8516563

KB Article ID# PL8516563

Contents

SummaryDetails

Associated Components