Solid Edge How to access Solid Edge basic File Properties dialog when using SEEC

2021-10-06T23:57:32Z
DOC_MANAGEMENT

Summary


Details

From time to time you may need to access the basic Solid Edge File Properties dialog when you are editing a Teamcenter managed Solid Edge file in the SEEC environment.  When selecting the File Properties command you are presented the SEEC File Properties dialog as seen below, but would like to display the basic File Properties dialog.



Solution

In order to display the basic Solid Edge File Properties dialog, you need only to select the following key sequence Ctrl+Shift+F to display the basic dialog as seen below.



Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V221.0
Function: SEEC

Ref: 002-8516430

KB Article ID# PL8516430

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC