Want to change position of Alternate Position assembly shown in drawing view.

2021-10-06T23:57:32Z

Summary


Details

Created an alternate position assembly and placed views in Draft of one of the positions. Now want to change the position on just one of the views to show the other position.

Solution

Right click on the view you want to change and select "Set Primary and Alternate Positions". This will bring up a dialog which will have the current member selected as the Primary. Just pick the desired member in the Primary column and OK the dialog, then update the view.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220MP8
Function: DRAWING_VIEWS

Ref: 001-9894687

KB Article ID# PL8516350

Contents

SummaryDetails

Associated Components