Solid Edge PCB Collaboration Add-on [SE364] missing from Solid Edge Premium

2021-10-06T23:57:29Z

Summary


Details

According to the Pricebook the Solid Edge PCB Collaboration Add-on [SE364] should be included with the Solid Edge Premium product:

However, I cannot see this PCB Collaboration Add-on in my Solid Edge session.  In the following screenshot the expected PCB tab with Solid Edge Premium is missing:

How do I get the Solid Edge PCB Collaboration Add-on [SE364] to work with my Solid Edge Premium license?

Solution

In order to be able to use the Solid Edge PCB Collaboration Add-on [SE364] with Solid Edge Premium you must first download and install a  separate piece of software, the Solid Edge PCB Collaboration Add-on:
 
Once this additional piece of software is downloaded and installed, the  Solid Edge PCB Collaboration Add-on will then be available in the Solid Edge Assembly environment when using a Solid Edge Premium license:




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: SE_PCB
Version: V220.0
Function: OTHER

Ref: 002-8515876

KB Article ID# PL8515876

Contents

SummaryDetails

Associated Components