CMM - Error while saving data to Teamcenter: The input string is too long.

2021-10-06T23:27:47Z

Summary


Details

Saving from NX to Teamcenter failed with error:


*** Partial Errors caught in Teamcenter PartialErrorListener. 
PARTIAL_ERROR_BEGIN 
[[3808*]] Thread. 
PartialErrors clientId= "26547;0" 
ErrorValues message="The input string is too long." Code:"515035" 
ErrorValues message="Unable to set value on property Finish Item." Code:"38048" 
ErrorValues message="Unable to set value on property ." Code:"38048" 
ErrorValues message="The Form "10238740/01" could not be saved." Code:"28009" 
PARTIAL_ERROR_END 



Solution

Description: 
The attribute in TC for “FINISH” only accepts up to 42 characters. 
The value in given example contains 50 characters. 


Solution: 
1) Change BMIDE and allow more characters for “FINISH” in TC. 
2) Disable NX manager mapping for “FINISH”. 
3) Clean up source data and shorten the entry. 



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 10_1809
Product: NX
Application: CMM
Version: V1899
Function: SWORKS

Ref: 001-9876358

KB Article ID# PL8515671

Contents

SummaryDetails

Associated Components