Not all tool parameters/attributes are available in Machining Knowledge Editor
2021-10-06T23:27:47Z
Summary
Details
When creating machining rules in MKE, not all tool parameters are available. For example the "Flute Length" attribute is available, but "Length" is not. Is there a way to add more attributes?
Solution
The MKE is showing the tool attributes from the Search Result dialog (RSET entry in def file). So it is possible to add more attributes by customizing this, even though they are not included by default. The following is an example how to add "Length" to Twist Drills:
1. Open ...\MACH\resource\library\tool\ascii\dbc_tool_ascii.def. 2. Because no db alias for the length exists, it must first be added ("HEI" is what the tool length parameter is called in tool_database.dat):
DB_ALIAS Length { DB_ID HEI DB_ID_TYPE d DIALOG_NAME "(L) Length" RSET_NAME "(L) Length" }
3. Scroll down to CLASS TWIST_DRILL and add the db alias "Length" to the RSET entry:
4. Save and close the file. 5. Start MKE. 6. File --> Open and Update. 7. Open machining_knowledge.xml. 8. Now the Twist Drill includes the Length attribute.
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: CAM Version: V1926 Function: FEATURE_BASED