How to add a new member (Bitmap) in the Structure Designer Stock?

2021-10-06T23:27:47Z

Summary


Details

Adding new components in the inventory for the Structure Designer Stock with pictures.

Solution


The stock list for the Structure designer can be found under ..\NXSTRUCTUREDESIGN\data\library\SectionReg.xlsx



First add a new directory named "Bitmap" ( Case sensitiv! )
under the directory "library", and put your bitmaps from your new Members under this directory.


Example :

Be sure that the Bitmaps are small . (e.g 150x150)

Example:


To define it in the "SectionReg" Excel, you should add suffix ".bmp", like "BR Profile 45×45{BR_Profile_45×45_mm.bmp},{ BR_Profile_45×45_mm_b.bmp }"

Notice: there are two pages in Excel (Shapes_in / Shapes_mm).

Make sure that the bitmaps and the real parts in this list are in the right places and that the bitmaps and the parts are in the right folder on the hard disk.
The names of parts and bitmaps must be identical in the Excel list and on the hard disk.




These steps will make it work to add bitmaps for customized types.






Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: STRUCTURE_DES
Version: V1934
Function: MEMBER

Ref: 002-8515565

KB Article ID# PL8515565

Contents

SummaryDetails

Associated Components