Solid Edge Failed to create a session object

2021-10-06T23:57:29Z
DOC_MANAGEMENT

Summary


Details

The Solid Edge Teamcenter Integration [SEEC} will not run and throws the following error message:
 
Failed to create a session object. Verify that your Solid Edge Teamcenter Client software installation and Solid Edge are the same Version and Maintenance Pack level.


Solution

This is a misleading error message.

The issue is actually that after updating the workstation to the Windows 10 version 2004, a Microsoft introduced operating system issue is then preventing SEEC from successfully running.
 
This issue can be overcome by downloading and installing the specific Microsoft KB4568831 fix:
 
https://support.microsoft.com/en-in/help/4568831/windows-10-update-kb4568831
 
By downloading and installing this specific Microsoft KB, this will then resolve the issue with SEEC not running and throwing this error message.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 002-8515486

KB Article ID# PL8515486

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC