LOV Property with the expected values is not displaying in the Common Properties dialog

2021-10-06T23:57:28Z

Summary


Details

When attempting to upload a file to the Teamcenter server the Common Properties dialog (CPd) does not display the LOV properties with the list of values that are expected.  There is no drop-down list of values to choose from. 

Solution

Make sure the attribute mapping definition file for the Solid Edge file type contains a section that is specific for the Teamcenter custom Item type.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1809
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 002-8515122

KB Article ID# PL8515122

Contents

SummaryDetails

Associated Components