NX Older NX versions could not locate the Java Virtual Maschine (JVM) Library

2021-10-06T23:27:47Z
NX System Administration

Summary


Details

When starting NX, this message comes up:

What exactly needs to be set?

Solution

The UGII_JVM_LIBRARY_DIR must point to the subfolder "server" inside the "bin" folder of the Java installation path:

e.g.:
UGII_JVM_LIBRARY_DIR=C:\Program Files\Java\jre1.8.0_261\bin\server

This is different to the UGII_JAVA_HOME which points to the folder of the Java installation, where the "bin"  subfolder is in:

e.g.:
UGII_JAVA_HOME=C:\Program Files\Java\jre1.8.0_261






Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V10.0
Function: INSTALL_ISSUES

Ref: 002-8515118

KB Article ID# PL8515118

Contents

SummaryDetails

Associated Components

Installation