Replacing the output of the Rapid Motion rap1, rap2 and rap3 variables in Post Builder
2021-10-06T23:27:47Z
Summary
Details
The X, Y and Z output for a G00 rapid move is output from the Program & Tool Path -> Program -> Motion -> Rapid Move rap1, rap2 and rap3 words. These words cannot be removed and the contents of the words are locked and cannot be edited. How can the output of these words be changed?
Solution
Use the Output Condition function to suppress the entire rap1, rap2 and rap3 line.
1. Uncheck the Work Plane Change option so that the rap1, rap2 and rap3 words are in the same line. 2. Add a new Output Condition to the line with a return 0 command to suppress the entire line. 3. Add a new XYZ line to replace the former rapid line.
Notes and References
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: NX Application: CAM Version: V1942 Function: POSTBUILDER