Question: Where do the PS on TC disconnected study files get extracted?

2021-10-07T00:01:56Z

Summary


Details

When loading a disconnected study for PS on TC Standalone, where do the disconnected study files get extracted? Does it clean up the files afterwards, or does the user have to do that? 



Solution

Here is how it works:

Version 15.1
1. PS extracts the psz-tc under a directory %TMP%\pvw<four-hex-digits>.tmp
2. Uses additional directory for what we call Engineering Data: %TMP%\ENG<four-hex-digits>.tmp
3. And often one more additional directory: %TMP%\SCR<four-hex-digits>.tmp

Note that the <four-hex-digits> part is different for the different directories. It is a sequence generated by Windows.
When the scene is unloaded (which when PS is closed or scene is loaded again), the above directories are automatically deleted by PS.

Version >= 15.1.2 and HF 47 of 15.1
There is a change in step 1 only.
Instead of %TMP%\pvw<four-hex-digits>.tmp, it goes under %LOCALAPPDATA%\Tecnomatix\PID.
Again, care is taken to delete the directories.
In addition, even if someone kills the PS process, on the next start PS will clean orphan subdirectories under %LOCALAPPDATA%\Tecnomatix\PID.

So, the directories would remain only if PS terminates abnormally. 



Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: 1064
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V15.1
Function: BACKBONE_INTEG

Ref: 001-9874679

KB Article ID# PL8515023

Contents

SummaryDetails

Associated Components