How to show invisible Network Drive in NX?

2021-10-06T23:27:47Z

Summary


Details

How to show invisible Network Drive in NX?
How can I configure the "EnableLinkedConnections" registry value to show the invisible Network Drive?.

Solution

To configure the EnableLinkedConnections registry value, follow these steps:


Step 1 :-  Go to Start, type regedit in the Start Search box, and then press ENTER.

Step 2 :-  Locate and then right-click the following registry subkey:


     HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\Current Version\Policies\System


Step 3 :-  Point to New, and then click DWORD Value.

Step 4 :- Type EnableLinkedConnections, and then press ENTER.

Step 5:-  Right-click EnableLinkedConnections, and then click Modify.

Step 6 :- In the Value data box, type 1, and then click OK.

Step 7 :- Exit Registry Editor, and then restart the computer.



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: xp64
Product: NX
Application: SYSTEM
Version: V12.0
Function: WNT_OS_ISSUES

Ref: 002-8514683

KB Article ID# PL8514683

Contents

SummaryDetails

Associated Components