Outputing Yes or No in a Work Instruction Cutcom Column

2024-03-13T14:55:40Z

Summary


Details

The variable mom_cutcom_type is used to report whether Cutcom is enabled for each operation in a Work Instruction(OWI) form. 0 is listed if it is turned off and 1 if turned on. A blank space indicates that operation type does not use Cutcom. Can the 0 and 1 be  changed to text output?


Solution

Open owi_template_operation_list.xlsx in Excel and add the text '${mom_cutcom_type:0='No';1='Yes';2='Yes';""} to a cell. The Excel file is published after the cell edit.


The OWI is next published from inside the CAM program file. The Cutcom status will be displayed as seen below. This text display is more intuitive than the number output.


Notes

Setting the Cell format to General will help with the output format.


Notes

KB Article ID# PL8514542

Contents

SummaryDetails

Associated Components