Some functions no longer available when fewer monitors are connected.

2021-10-07T00:01:56Z

Summary


Details

When the laptop is connected with two external monitors, everything works fine.

After closing Process Simulate, one of the monitors was removed.

Now things are not working correctly.  When trying to open different functions, just hear a "Ding" and nothing happens.

Solution

This sounds like there is a dialog open, but it is outside the current viewable area.

To reset the positions of everything in Process Simulate:


  1. Close any open sessions of Process Simulate.
  2. Open the Tecnomatix Doctor utility.  (Start / Tecnomatix / Tecnomatix Doctor)
  3. Look under the Tools pulldown menu.  There should be an entry called "Reset Dialog Position".
  4. Invoke this, then restart Process Simulate.
         Note: You may need to run this with administrator privileges.

Hardware/Software Configuration

Platform: na
OS: windows
OS Version: 10_1709
Product: TECNOMATIX
Application: PROCESS_SIMULAT
Version: V15.0.1
Function: TOOLS

Ref: 002-8514458

KB Article ID# PL8514458

Contents

SummaryDetails

Associated Components