Robot will not initialize, receiving error -68 from RCS.
Solution
This Virtual Robot requires a weight be attached by default . The virtual robot must be modified during creation to turn off the check for a weight.
So, when creating the virtual robot in the Fanuc Virtual Robot Setup Wizard, check "Stop at Controlled Start" checkbox on the last dialog screen; when it stops, select "m" for Menu.
In the Menu, select "4" for Variables.
Cursor key down the list to 737. Use the F5 key to change it to FALSE.
Press "f" key, then Enter key to resume the Virtual Robot creation.
Notes and References
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: TECNOMATIX Application: PROCESS_SIMULAT Version: V15.1 Function: OLP_CONTROLLERS