What is the Jurisdiction and Classification of the NX software itself, per U.S. export regulations?
Solution
From the Export Compliance board:
NX Software is subject to the EAR (US technology). It's classified as EAR99.
NX as a platform is classified as EAR99 (subject to EAR).
However some NX add-on products have different ECCN classifications.
Siemens is not in the position to provide or advise our customers on export control topics.
The following information should be sufficient for the customer to properly assess their export control restrictions:
NX software family is classified with ECCN= EAR99 under the EAR.
P/N TC30600 is classified at a higher level as it follows the classification of the Teamcenter product family.
ECCN for Teamcenter = 5D002.c1 under the EAR (classified by the BIS under CCATS# G046771)
"This encryption item is authorized for license exception ENC under sections 740.17 (A) and (B) (3) of the Export Administration Regulations."
Notes
Notes