How to disable auto work part change in NX assemblies
2021-10-06T23:27:46Z
Summary
Details
How to disable Work Part change when selecting components in assembly context?
Solution
In order to have the "Allow Automatic Work Part Change" toggle be available the user must first set the Customer Default Modeling-> General-> General tab-> "Allow Automatic Work Part change" on.
Once it is set and NX is restarted, the user will now be able to toggle that behavior on or off with the following icon
Notes and References
Hardware/Software Configuration
Platform: na OS: all OS Version: n/a Product: NX Application: SYSENG Version: V1926 Function: SELECTION