Solid Edge Teamcenter returned 000000008004A008 which SEEC does not recognize as a known error

2021-10-06T23:57:26Z
DOC_MANAGEMENT

Summary


Details

One of our customer's users receive this error message when opening a part from Teamcenter or when closing/saving to Teamcenter.


This happens for all parts, drafts and assemblies, but only for this one user.


The full error message reads:


Teamcenter returned 000000008004A008 which SEEC does not recognize as a known error. Review the log file for further information.

The problem is user specific, other users are able to open the same files without an error


How to resolve this error?



Solution

To resolve this issue, in Teamcenter clear all the values for the following Teamcenter preferences by using Teamcenter --> Edit --> Options--> Search:


  • MyHistory 
  • myfavorites 
  • MySearchHistory


Restart Teamcenter and the Solid Edge sessions.

With the preferences cleared and the sesion restarted the issue is now resolved.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220.0
Function: SEEC

Ref: 001-9858480

KB Article ID# PL8514170

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC