Solid Edge Decimal delimiter for Mass does not correspond with local settings

2021-10-06T23:57:25Z
DOC_MANAGEMENT

Summary


Details

Mass is mapped to a Teamcenter property type "Double".  If the user has defined in Windows a comma as decimal separator the attribute is not synchronized to Teamcenter.  In contrast, with the point as decimal separator it works.







Solution

In this case the used attribute mapping was the problem.  The user did not include the "Item type" in their mapping.

e.g:

{ Dataset type="SE Part"
          "Mass" : ItemRevision.a3Weight /master=cad /description="model weight"
}

For Solid Edge this mapping is not correct, it requires the inclusion of the "Item type".  The issue is fixed by changing the attribute mapping to the following:

{ Dataset type="SE Part"
     {Item type="Item"
               "Mass" : ItemRevision.a3Weight /master=cad /description="model weight"
     }
}

Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP8
Function: SEEC

Ref: 002-8513886

KB Article ID# PL8513886

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC