NX nxmgr, opening jt, object doesn't exist

2021-10-06T23:27:46Z
NX for Design

Summary


Details

  - In NX Manager, unable to open a DirectModel dataset.
  - Error message of
      Error - object does not exist.


  - NX syslog shows

*** EXCEPTION: Error code  920002 in ...\ui_ugmgr_part_input.c ...
+++ Failed to open OS file ...



Solution

  - In Teamcenter, the value for the preference
      TC_NX_Foreign_Datasets

    had the wrong double quote character.

  - After *typing* in the value

DatasetType="DirectModel" NamedReference="JTPART" NamedReferenceFormat="BINARY" NamedReferenceTemplate="jt"

    for this preference, File --> Open in NX/Manager was successful.




Notes and References

  If you prefer to copy and paste, you may want use Notepad,
  instead of MSWord file or PDF file.

  You may also see the following multicad error

   The following files could not be loaded, causing this open to fail:
      ... (multi-CAD: ..) - The multi-CAD dataset is empty; create or import some data and try again.



Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1926
Function: FILE_OPEN

Ref: 002-8513881

KB Article ID# PL8513881

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX