Want to change all dimensions in a file from Inch to mm.

2021-10-06T23:57:24Z

Summary


Details

Want to change all dimensions in a file from Inch to mm.



Solution

The easiest way is to go into the style being used in that file for the dimensions, go to the Units tab and change it to mm there. This might be confusing, though, if the style is "ANSI (inch)" and shows up as metric in that file. You could also use SmartSelect to pick all dimensions on a sheet and change them with Edit Properties to a different style (ANSI (mm), for example).



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220MP8
Function: STYLES

Ref: 001-9858567

KB Article ID# PL8513737

Contents

SummaryDetails

Associated Components