Simcenter 3D Solutions Simulate particle flow through a screen.

2021-10-06T23:27:46Z
Simcenter 3D

Summary


Details

I would like to simulate particle flow through a screen.

In the screen setting, only the free area ratio of thin perforated plate can be defined. 

How do I know if the particle is able to flow through the screen as the hole diameter 

and the number of holes cannot be input?

Solution

When defining the Screen simulation object, turn on the "Pass-Through" toggle to obtain a report on the number of particles passing through the screen.

The free area ratio is used to calculate a head loss coefficient at the screen. However, it is not used to determine whether the particles are trapped by the screen based on a comparison between the perforation and particle diameters.  

Notes

KB Article ID# PL8513684

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow