Setting the units for Mass Moments of Inertia

2021-10-06T23:57:24Z

Summary


Details

Where are the units set for the Mass Moments of Inertia?



Solution

The Units for the Mass Moments of Inertia is set by the Derived Units "Density" Value in the Solid Edge Options > Unit Tab. 

You can reach the "Units" Tab via any of the following methods:


  • Application Button > Info > File Units- Quick Access Tab (QAT) > Options 
  • Application Button > Setting > Options
  • Application Button > Info > File Properties > Units Tab > Click Solid Edge Options > Units Button 

Each method opens the Solid Edge Options Dialog which contains the Units Tab with the available Units settings.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V220MP8
Function: OPTIONS

Ref: 001-9854597

KB Article ID# PL8513618

Contents

SummaryDetails

Associated Components