How can we export UGALTREP by "ug_clone"?

2021-10-06T23:27:46Z

Summary


Details

How can we export UGALTREP by "ug_clone"?



Solution

Use the below syntax for the data containing the UGMASTER, AltRep, and UGPART dataset. Refer below snap-
 



 
 
ug_clone -pim=yes -u=infodba -p=infodba -g=dba -o=export -default_n=autotranslate -copy_n=specification:yes -default_d="C:\IR_Data\Export\3" -asse=@DB/000621/A -s=C:\IR_Data\Export\3\export_log.clone
 
 
After Export below is the format I have received for the part file created  -
 

 
 
After Export the data is exported as mentioned below- 
 
Master Dataset -000621_A.prt (ItemID_RevisionID)
Non-Master Dataset - 000621_A_s_Test-A-dwg.prt (ItemID_RevisionID_Specification/Relation_Datatset Name)
Non-Master Dataset - 000621_A_a_Test-A-dwg.prt (ItemID_RevisionID_Specification/Relation_Datatset Name)

Notes and References

9727621



Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: CLONE_EXPORT

Ref: 002-8513598

KB Article ID# PL8513598

Contents

SummaryDetails

Associated Components