NX Leader stub of PMI FCF differs in drafting scaled views

2021-10-06T23:27:46Z
NX for Design

Summary


Details

The PMIs do not honour the same alignment as in modeling when placed in drafting with any scale other than 1:1. 
-------------------------------------------------
Steps
1. Add a feature control frame(or a note) in any modeling view
2. Go to drafting
3. Add the same view in drafting with any scale other than 1:1 ( e.g. 1:2 )
4. You will notice that the alignment of FCF is disturbed.

Solution

This is a current designed behaviour.
The reason behind this is that we do not have mechanism to scale the origin based on the view scale.
 
For example the model PMI has text height 3.5 as shown below
And in (0.5) scaled view, the size of the text height is 3.5 * (1 / 0.5) = 7 to match the display. So, the bounding box is changed. Hence the leader stub differs.


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: PMI
Version: V1867
Function: DIMENSION

Ref: 002-8513591

KB Article ID# PL8513591

Contents

SummaryDetails

Associated Components

PMI