NX PMI section view is not exported as displayed in graphics screen in PDF, CGM.

2021-10-06T23:27:46Z
NX for Design

Summary


Details

PMI section view is not exported as displayed in graphics screen in PDF,CGM
The portion that is cut by section view also visible in the exported PDF,CGM
However Legacy PMI section view works correctly

Solution

This is the current limitation of dynamic section and not specific to 
Lighweight section but its true even in case of PMI Sections.
But now with the Technical Data Package (TDP) ,users can create 3D PDFs wherein user can see the PMI Section View and visualize it in 3D PDF.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: PMI
Version: V1872
Function: SECTION_VIEW

Ref: 002-8513590

KB Article ID# PL8513590

Contents

SummaryDetails

Associated Components

PMI