How to set PMI decimal places in customer defaults?
2021-10-06T23:27:46Z
Summary
Details
Though we could set Decimal places for PMI dimensions from PMI preferences, we could not set the same from customer defaults. How to set PMI decimal places in customer defaults?
Solution
This setting is controlled by the corresponding drafting settings in customer defaults. After setting the above and restarting NX, the changes will be reflected only in the new files that are created from a blank template as the scope of this setting is "part".
If the user expect the setting should be reflected in model template as well, he/she need to follow the below steps.
1.Set the needed setting in customer defaults. 2.Create a new part from blank template. 3.Create a Datum CSYS same like model template 4. Save the part as "model-plain-1-mm-template.prt" 5. Replace the model template part from NX installed folder \NX1926\UGII\templates with the saved one in step 4 6. Restart NX
Hardware/Software Configuration
Platform: INTL64 OS: windows OS Version: 1064 Product: NX Application: PMI Version: V1847 Function: DIMENSION