Simcenter 3D Solutions Acoustic absorber in SOL107

2021-10-06T23:27:45Z
Simcenter 3D

Summary


Details

In SOL108/111, the function is used for modeling acoustic absorption on walls.

 In SOL107, Does the acoustic absorber will act as absorber in the same way as SOL108/111?

Solution

If you are defining absorber in following way then the behaviour should be same.

The Acoustic Absorber  corresponds to the Nastran CAABSF  and PAABSF  bulk data entries. 

Supported NX Nastran solutions 

The following solution types are supported with both acoustic and vibro-acoustic solutions: 

•SOL 103 – Real Eigenvalues 

•SOL 107 – Direct Complex Eigenvalues 

•SOL 108 – Direct Frequency Response 

•SOL 110 – Modal Complex Eigenvalues 

•SOL 111 – Modal Frequency Response 

In order to specify an absorbing boundary condition (which AML also is) for SOL107, it is best to use a PAABSF with the impedance set to the characteristic impedance of the outside fluid (rho.c).

Notes

KB Article ID# PL8513571

Contents

SummaryDetails

Associated Components

Acoustics Additive Manufacturing Assembly FEM Correlation and Updating Durability Electromagnetics (High Frequency) Electromagnetics (Low Frequency) Flexible Pipe Laminate Composites Margin of Safety Motion Multiphysics NX Open Nonlinear Optimization Pre/Post Response Dynamics Rotor Dynamics Samcef Environment Simulation Process Management Thermal / Flow