Solid Edge Custom Material is conflicting with Solid Edge material.

2021-10-06T23:57:24Z
DOC_MANAGEMENT

Summary


Details

When you try to apply a value in the Properties dialog, the following message comes up:


"A file property already exists with the same name as the custom file property you have added, named material."



Solution

'Material' is a reserved Solid Edge Property. This prohibits the use of 'Material' as a custom property. If this condition already exists in the Solid Edge document, the custom Material property name needs to be changed so it  does not conflict with the Solid Edge Material property name.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 10_1909
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V220MP8
Function: SEEC

Ref: 001-9847700

KB Article ID# PL8513495

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC