NX How to create additional top nodes under Routing part library?

2021-10-06T23:27:45Z
NX for Design

Summary


Details

How to create additional top nodes under Routing part library?

Solution

It is not possible to have additional top nodes under Routing Part library.
 
That's the limitation. However users can rename existing top nodes to desired names as he/she wishes.
 
Or else users can add additional sub nodes
 
For e.g.  The user can rename the existing one to "All Parts" and under that he/she can have his own sub-nodes along with existing nodes as shown below
 


Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: NX
Application: ROUTING_GENERAL
Version: V12.0.2
Function: REUSE_LIBRARY

Ref: 002-8513476

KB Article ID# PL8513476

Contents

SummaryDetails

Associated Components

Routing