NX Make a Component Group use Boolean as component attribute.

2021-10-06T23:27:45Z
NX for Design

Summary


Details

At the component level, I create these attributes:

At the assembly level, I can create a component group under, "Component Groups in Part" folder by selecting "Component Groups in Part" folder --> RM --> Add to Component Group --> By Attribute -->Type
attribute name, Boolean, Integer, or String, then type the value as shown above.

After toggling on each group, you would see the count as below in ANT:
Notice String and Integer correctly display the count (1), however Boolean doesn't display it correctly, (0).
How can you correct this?



Solution

In the "Add Component Group" dialog , the Component Attribute's value needs to be lower case,
so component attribute was created as "True" or "False" need to be "true" and "false".

You might need to toggle the group off and on for it to display correctly, but it should be correctly displayed as below:






Notes and References


Hardware/Software Configuration

Platform: na
OS: windows
OS Version: n/a
Product: NX
Application: ASSEMBLIES
Version: V1926
Function: ASSEMBLY_MODEL
Product: NX
Application: ASSEMBLIES
Function: ASSEMBLY_MODEL

Ref: 001-9848122

KB Article ID# PL8513391

Contents

SummaryDetails

Associated Components

Assemblies