Can't save to eMS

2021-10-07T00:01:55Z

Summary


Details

Cannot save data to eMS.  Error:  Data will not save.



Solution

Import the Robotics Customization.

1)  If a project is open in Process Simulate, it must be closed before you can import another project.
2)  All data contained in the project is imported as checked out.
3)  It is recommended that all data be checked in before you start working on the project.
4)  Choose File tab → Import/ExportImport Customization.
5)  Select the folder in which the robotics customization is located.
6)  Select OK.



Hardware/Software Configuration

Platform: na
OS: windows
OS Version: 10_1809
Product: TECNOMATIX
Application: EM-SERVER
Function: EM-SERVER

Ref: 002-8513386

KB Article ID# PL8513386

Contents

SummaryDetails

Associated Components