NX Setting up environment variable to import/export part familes

2021-10-06T23:27:45Z
NX for Design

Summary


Details

What is the variable that allows part families members to be imported/exported from Managed NX?

Solution

UGII_UGMGR_ALLOW_PFM_IMPORT_EXPORT = 1

Used for family members with no templates when importing and exporting assemblies. If the variable is not set then the family members will not be imported into portal. If the variable is set, then it will be given precedence over UGMGR_CloneImportExportAutoRemovePFM. When an assembly referencing part family members is imported/exported, there will not be any change to the existing behavior. The required part family members will be automatically generated during this process.




Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: GATEWAY
Version: V1926
Function: CUSTOMER_DEFS

Ref: 002-8513372

KB Article ID# PL8513372

Contents

SummaryDetails

Associated Components

Modeling