Details
When NX goes to continuous release, what is the impact on Teamcenter RAC and particularly the start_nxmanager.bat. file in the portal directory?
In that file there is a ugs_router command with a "-version" argument that indicates which installed version of NX to use.
How will that be impacted in an environment of either selecting the automatic updates for NX or manually pushing the updates for NX.?
Solution
When upgrading a "series", such as 1847, 1872, 1899 (similar to blockpoint releases), NX will install into a new folder. In these cases, it will be necessary to run the Teamcenter Environment Manager (TEM) and remove the NX Rich Client feature, and then run TEM again and reinstall it. It will prompt for the new NX path,.
In the case of a "patch" (previously referred to as an MP), the installation will modify the existing "series" files and the path will remain the same.
Hardware/Software Configuration
Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V1847
Function: STARTUP
Ref: 002-8513371