How to unite multiple bodies in a single solid with no parameters

2021-10-06T23:27:44Z

Summary


Details

Imported STEP file created multiple solid bodies. Need to combine them all into a single solid with no parameters.



Solution

To produce a single solid body with no parameters:
1. Select Menu->Insert-> Combine-> Unite. 
2. Select an initial imported STEP solid body as the Target and select the remaining solid bodies as the Tool bodies. OK to Unite all the bodies to a single solid body 
3. Select Menu-> Edit-> Feature-> Remove Parameters and select the United body in the work area. OK.
This removes parameters from the United bodies and deletes the original un-parameterized bodies so only a single solid remains in the Part Navigator and in the Work Area. 



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: FEATURE_MODEL

Ref: 001-9853941

KB Article ID# PL8513272

Contents

SummaryDetails

Associated Components