The connection mode between Solid Edge Wiring and Harness design and Solid Edge Routing does not start
2021-10-06T23:57:24Z
Summary
Details
When the customer tries to use the connection between Solid Edge Wiring and Harness Design (SEWHD)and Solid Edge Routing the error message appears : Retry by running Solid Edge as administrator.
Solution
The application uses a web service in Connect Mode between SEWHD and Solid Edge Routing. This Web Service has to be run in Administrator mode otherwise the web service is not started. In non-administrator mode, the services from the Solid Edge application are not started and the following message is displayed to the user: Retry by running Solid Edge as administrator
For establishing a connection between Solid Edge & Solid Edge Electrical, Solid Edge has to be launched in Administrator mode.
Hardware/Software Configuration
Platform: all OS: n/a OS Version: n/a Product: SOLID_EDGE Application: SE_ELECTRICAL Version: V220MP1 Function: CONNECTED_MODE