How to install 'Mold Tooling' silently?

2021-10-06T23:57:23Z

Summary


Details

The administrator of a customer wants to easily install 'Mold Tooling' on several machines and asks for a way to execute a silent installation of this product.

Solution

The following steps describe how this silent installation can be executed on top of an existing installation of Solid Edge.

1. Download the appropriate language-specific executable from the Siemens PLM Download Server (e.g. Solid Edge > Full products > Windows (64-bit) > 2020 > Portfolio Products > Mold Tooling >  MoldTooling_2020_ENGLISH.exe)

2. Extract the executable e.g. with 7-Zip.

3. Run a 'Command Prompt' as Administrator.

4. In this command prompt change to the directory where the executable was extracted to.

5. Change to the directory 'Mold Tooling' (it contains the Siemens Solid Edge Mold Tooling 2020.msi).

6. Enter the following exemplary command to start the silent installation:

msiexec /i "Siemens Solid Edge Mold Tooling 2020.msi" /qn+ /l*v "D:\temp\se_mold_tooling_de.log"

Note: Please adjust the path and the name of the log file (e.g. D:\temp\se_mold_tooling_de.log).

7. Wait for and then close the message that reports success.

8. Check the created log file if needed.

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: MOLD_TOOLING
Version: V220.0
Function: MOLD_TOOLING

Ref: 002-8512886

KB Article ID# PL8512886

Contents

SummaryDetails

Associated Components