ProE Data Migration is interrupted with the message: Creo Toolkit application "UNNAMED" was not unlocked

2021-10-06T23:57:23Z

Summary


Details

After starting the ProE Data Migration process Creo Parametric starts and suddenly interrupts the process with the following message:



The ProE Data Migration log window simultaneously shows the message: "Could not start ProE session on ProE host. Either ProE is not installed on the specified ProE host or ProEStartUpFile entry in INI file is not correct."  It also documents the termination of the migration.

Solution

Close the "UNNAMED" message (it will end the Creo Parametric session as well) and close the ProE Data Migration log window.

Execute the following steps to unlock the Creo Toolkit application:


  1. Open an Administrator Command Prompt
  2. Change the directory to <PTC_PATH>\<CREO_VERSION>\Parametric\bin (e.g. cd /d "D:\apps\PTC\Creo 5.0.4.0\Parametric\bin")
  3. Unlock the application with the command: protk_unlock.bat "<SOLID_EDGE_PATH>\Program\ProESEServerSide.dll" (e.g.: protk_unlock.bat "C:\Program Files\Siemens\Solid Edge 2020\Program\ProESEServerSide.dll")
  4. Note the message of success: "... Successfully unlocked application."


Close the Command Prompt window and repeat the ProE Data Migration. It should now work as expected.

Notes and References

If the situation sporadically reoccurs the following commands entered in a batch file will help to easily redo the unlock task.

@echo on
cd /d "D:\apps\PTC\Creo 5.0.4.0\Parametric\bin"
call protk_unlock.bat "C:\Program Files\Siemens\Solid Edge 2020\Program\ProESEServerSide.dll"
pause

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: TRANSLATORS
Version: V220MP8
Function: PROE

Ref: 002-8512689

KB Article ID# PL8512689

Contents

SummaryDetails

Associated Components