'Links' dialog does not offer the 'Break Links' command for assembly and draft documents

2021-10-06T23:57:22Z

Summary


Details

If a part document with a link to another file is opened in Solid Edge the 'Links' dialog (Application Button > Info > Edit Links) shows a 'Break Links' button to disconnect the link from the source file.  

If an assembly or a draft document with a link to another file is opened, the 'Links' dialog does not offer this 'Break Links' button.  Therefore how can any links be deleted/removed in assembly and draft documents?

Solution

Links in assembly and draft documents can be removed through the 'Binder' dialog (Application Button > Info > Binder).  After selecting the linked document in this dialog, hit the 'Delete' key and when prompted with "Delete the selected object?" question, click the 'Yes' button to remove the link. 

Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V220.0
Function: OLE
Product: SOLID_EDGE
Application: ASSEMBLY
Version: V220.0
Function: OLE

Ref: 002-8512672

KB Article ID# PL8512672

Contents

SummaryDetails

Associated Components