Solid Edge The Solid Edge Standard Parts database behaves very slow

2021-10-06T23:57:22Z
APPLICATION

Summary


Details

When the user wants to place a standard part or the administrator uses the Standard Parts Administrator tool to work with the database, the database reacts very slow.



Solution

The most common culprit is that users add all available standards into their database. That is not best practice and mostly not necessary.

Currently, we offer the following standards.


  • ANSI - American
  • ASME - American
  • BS - British
  • CSN - Czech
  • CNS - Chinese
  • DIN - German
  • GOST - Russian
  • GB - Chinese
  • IS - Indian
  • ISO - International
  • JIS - Japanese
  • KS - Korean
  • UNI - Italian


To keep the database as small and as fast as possible make sure to delete all standards your company does not need.

Respectively from the initial install only load those parts and standards that are needed. Bear in mind you can add missing parts, categories, or standards at any time.




Hardware/Software Configuration

Platform: INTL64
OS: windows
OS Version: 1064
Product: SOLID_EDGE
Application: APPLICATION
Version: V220.0
Function: STANDARD_PARTS

Ref: 002-8512590

KB Article ID# PL8512590

Contents

SummaryDetails

Associated Components

APPLICATION: STANDARD_PARTS