After SEWHD SP2002 maintenance pack installation the application does not launch

2021-10-06T23:57:21Z

Summary


Details

After installation of maintenance pack SP2002 for Solid Edge Wiring and Harness Design (SEWHD), the application does not start.  Before installing the maintenance pack it worked correctly.






Solution

 Check the license file:
 
 PACKAGE SEWIRHAR ugslmd 2.0 COMPONENTS="SEWIRHAR_seelecharness \ 
 SEWIRHAR_seelecwiring" OPTIONS=SUITE ck=203 SIGN="01DB 25B1 \ 
 
In this example the increment feature reported is ugslmd 2.0, which means that the license file is not updated for the installed SEWHD version.

It will be necessary to request a new license file where the increment feature will be ugslmd 220.0.



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: SE_ELECTRICAL
Version: V219MP6
Function: OTHER

Ref: 002-8512587

KB Article ID# PL8512587

Contents

SummaryDetails

Associated Components